MPC5602 and MPC5605 Compatibilty

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5602 and MPC5605 Compatibilty

997 Views
dipakpatil
Contributor II

Hello,

 

We are currently using the MPC5602 device for ongoing programs. But we are shifting to MPC5605 and/or MPC5606B due to memory requirements.

 

So are these two devices( MPC5602 and MPC5605) are compatible from SW point of view ? Means may I use the old SW (MPC5602) on the new device MPC5605 ?

 

Thanks,

Dipak

Labels (1)
3 Replies

841 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

First it would be needed to check whether you are using MPC5602B or MPC5602D.

Basically there are 4 different sub-familes where slight differences may exist but all these devices are very similar:

- MPC5602/3/4B and MPC5602/3/4C

- MPC5601/2D

- MPC5605/6/7BF

- MPC5605/6BK

I could recommend to see following documents: http://cache.nxp.com/files/32bit/doc/app_note/AN4036.pdf

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4477.pdf

http://cache.nxp.com/files/32bit/doc/app_note/AN4093.pdf

841 Views
dipakpatil
Contributor II

Hello David Tosenovjan

currently using MPC5602BF1MLL and shifting to MPC5605B or MPC5606B. Please comment

0 Kudos

841 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Following document compares MPC5604B family (that is MPC5602/3/4B and MPC5602/3/4C) and MPC5607B (that is MPC5605/6/7BF)

http://www.nxp.com/files/32bit/doc/app_note/AN4340.pdf

If you choose MPC5605/6BK variant you could also pay attention to this appnote:

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4477.pdf