MPC555 3V I/O Drive Strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC555 3V I/O Drive Strength

Jump to solution
1,709 Views
mohammak
Contributor II

Looking at MPC555 / MPC556 datasheet for I/O drive strength in page 64, a strength of 25/50pF is mentioned for 3V pins.

This is confusing because I cant confirm whether 25pF strength is for MPC555 and 50pF strength is for MPC556,

OR

25pF is half strength and 50pF is full strength for both MPC555/MPC556,

Can you please explain.

Thanks

0 Kudos
Reply
1 Solution
1,697 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.

As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.

Regards,

Lukas

View solution in original post

1 Reply
1,698 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.

As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.

Regards,

Lukas