MPC555 3V I/O Drive Strength

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC555 3V I/O Drive Strength

ソリューションへジャンプ
865件の閲覧回数
mohammak
Contributor II

Looking at MPC555 / MPC556 datasheet for I/O drive strength in page 64, a strength of 25/50pF is mentioned for 3V pins.

This is confusing because I cant confirm whether 25pF strength is for MPC555 and 50pF strength is for MPC556,

OR

25pF is half strength and 50pF is full strength for both MPC555/MPC556,

Can you please explain.

Thanks

0 件の賞賛
1 解決策
853件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.

As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.

Regards,

Lukas

元の投稿で解決策を見る

1 返信
854件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

the only difference between MPC555 and MPC556 is that MPC556 supports code compression. Other characteristics are exactly the same.

As you mentioned, 25/50pF means 25pF for reduced drive strength and 50pF for full drive strength.

Regards,

Lukas