MPC5500 & MPC5600 Family

cancel
Showing results for 
Search instead for 
Did you mean: 

MPC5500 & MPC5600 Family

724 Views
olegivanus
Contributor III

Hello, all.

I learn the organization of interrupt handlers on MPC5643L, but examples are few and I do not quite understand. In Qorivva Simple Cookbook MPC5643L not mentioned.

 

Tell me whether or not MPC5643L microcontroller relates to the family MPC5600?

If so, why in the table examples listed (AN2865 http://cache.freescale.com/files/32bit/doc/app_note/AN2865.pdf?fpsp=1)  present MPC56xxB/P/S MCU's but there is no -L?


Thank you

Labels (1)
0 Kudos
1 Reply

269 Views
petervlna
NXP Employee
NXP Employee

Hi Oleg,

Yes, Leopard MPC5643L is part of MPC56xx family. Seems to me like AN2865 is older and Leopard was most probably not included in portfolio when revision 1 of AN2865 came out. Most probably the table in AN2865 is outdated.

If you look at actual MPC56xx portfolio, there are many new controllers these days: Qorivva MPC56xx

0 Kudos