I have an assignment for a interview to do a high level design for a MPC5200 and a DDR2 interface. According to the data sheet the MPC5200 only supports DDR not DDR2. So is this possible to use DDR2 with the MPC5200 processor?
It is not possible,
Power supply for DDR is 2.5V.
Power supply for DDR2 is 1.8V.
Have a great day,
Pavel Chubakov
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------