MPC5125 Power on Reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5125 Power on Reset

跳至解决方案
4,395 次查看
luigibenciolini
Contributor I


In reference to a CPU board equipped with NXP MPC5125YVN400 we  found a malfunction at startup reset (PORESET)

The problem involves the boards equipped with processor with marking code QAT1535C.

Currently no problem are found on boards equipped with processor with marking code DAR1532AF.

 

Extending the reset time from 180mS up to 220mS (or more) the problem disappear; --> consider that the datasheet don't impose any constraint regarding the PORESET timing  (Obviously is requred that PORESET can be released after all the supplies reach the specified operating conditions).

 

Enclosed you find some oscilloscope screenshot

 

Thank You nn advance

Luigi

标签 (1)
1 解答
4,177 次查看
Pavel
NXP Employee
NXP Employee

Usually similar behavior detected if the following happens on the board:

power supply is not stable,

the MPC5125 PLL is not locked

the MPC5125 reset configuration incorrectly read.

Look at the Figure 5 of the MPC5125 Datasheet.

Is there the same behavior of the HRESET and SRESET on your board during power up?

Look at the Figures 51 and 52 of the MPC5125 Datasheet.

Do you use similar connection on your board?

If the second short PORESET is solution of your problem, power supply is not stable or the MPC5125 PLL is not locked during 182ms.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
4,178 次查看
Pavel
NXP Employee
NXP Employee

Usually similar behavior detected if the following happens on the board:

power supply is not stable,

the MPC5125 PLL is not locked

the MPC5125 reset configuration incorrectly read.

Look at the Figure 5 of the MPC5125 Datasheet.

Is there the same behavior of the HRESET and SRESET on your board during power up?

Look at the Figures 51 and 52 of the MPC5125 Datasheet.

Do you use similar connection on your board?

If the second short PORESET is solution of your problem, power supply is not stable or the MPC5125 PLL is not locked during 182ms.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,177 次查看
luigibenciolini
Contributor I

Pavel,

Thank you  for quick and useful answer.

Regarding your questions, the answer are:

1) The beahvior of HRESET and SRESET is congruent to that one showed in figure 5 (and Table 19) anyhow (both when the board starts correctly or not)

2) The connection of our schema is the same to that reported in figure 52

Other informations:

3) In effect +1V8 is not monotonic during rise time.

We tried to supply externally in order to guarantee monotoniticy but the problem  is not solved.

However, there is still a violation in the slew rate of the power supplies (faster than required in datasheet §.5.1=max 12V/ms).

I'll try as soon as possible also to reduce the power supply slew rate and repeat the test.

The Sequencing is correct (VDD core last)

4)The current workaround that we implemented is to enable the internal watchdog  before than the processor address to the DDR2. With this workaraound the "problematic" board starts correctly for more than 400 times (test executed with automatic equipment).

Luigi

As anticipated in the previous point 3), we tried to supply the CPU with a new DCDC stage with soft start in order to guarantee the slew rate less than 12V/ms.

The board now works fine. So I confirm that the problem was the violation of the power supply slew rate.

Luigi

0 项奖励
回复