MPC 5744P Compile difference of different SD32 version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC 5744P Compile difference of different SD32 version

Jump to solution
1,848 Views
TerryDuPower
Contributor III

Dear supporters:

      I created two project with some code. One was created by S32 Design Studio for Power Architecture Version 2017.R1, Another was created by S32 DS 2.1.   After complied, It's strange they are different.

 S32 DS 2017.R1:

TerryDuPower_1-1650247101857.png

 

S32 DS 2.1:

TerryDuPower_0-1650246970941.png

I checked the propertity is same . Could you give me some help?

0 Kudos
Reply
1 Solution
1,723 Views
TerryDuPower
Contributor III

Hi  stanish,

     Yes, It's caused by the compiler option  

-fstrict-volatile-bitfields

  

Thanks very much!

View solution in original post

0 Kudos
Reply
6 Replies
1,827 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Do you have the same linker file? Do you have same optimization configuration?

0 Kudos
Reply
1,799 Views
TerryDuPower
Contributor III

Yes,  two projects have same link file and same optimization configuration.

0 Kudos
Reply
1,766 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Can you provide your project or reproducible code snippet? Thanks

0 Kudos
Reply
1,759 Views
TerryDuPower
Contributor III

This is the code:  

void Tim_Init(void)
{
//STM_0.CR.R = 0x00003103;
STM_0.CR.B.FRZ = 1; /*0:STM counter continues to run in debug mode*/
STM_0.CHANNEL[0].CMP.R = 1000; /*matches the STM_CNT register*/
STM_0.CR.B.CPS = 0x31; /*counter prescaler */
STM_0.CR.B.TEN = 1; /*Timer counter Enabled*/
STM_0.CHANNEL[0].CCR.B.CEN = 1; /* channel 0 enable */
STM_0.CHANNEL[0].CIR.B.CIF = 1; /* clear the flag */
}

Thanks!

0 Kudos
Reply
1,736 Views
stanish
NXP Employee
NXP Employee

Hello,

it seems the difference is caused by the compiler option:

-fstrict-volatile-bitfields

this causes the bitfield struct access (peripheral register) respects the declared datatype.

See se_stw vs. se_stb instruction

In a previous version of the compiler this option was enabled by default. Later compiler versions (starting with v1.2+) this option has to be enabled expicitly in compiler options.

 

stanish_0-1651137824153.png

 

hope it helps.

Stan

 

0 Kudos
Reply
1,724 Views
TerryDuPower
Contributor III

Hi  stanish,

     Yes, It's caused by the compiler option  

-fstrict-volatile-bitfields

  

Thanks very much!

0 Kudos
Reply