MPC 5500 & 5600, LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,725件の閲覧回数
mateuszolsztyn
Contributor II

Hi all,

 

im using mpc5643L microcontroller and i want to display something. Can i use to it graphical LCD from Nokia 3310 (pcd8544)? Is it possible? Or can You recommend me something else?

 

Thanks & Regards

Mateusz

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,495件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

This LCD uses simple SPI bus (/SCE, SCLK, DIN) and some general inputs pins to control the display. So it can be easily controlled by any MPC5xxx MCU, the MPC5643L for sure. Only the driver have to be written by you. But you can find many examples for Nokia 3310 LCD handling on the web, so you can easily tailor it to your MCU.

BR, Petr

元の投稿で解決策を見る

2 返答(返信)
2,496件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

This LCD uses simple SPI bus (/SCE, SCLK, DIN) and some general inputs pins to control the display. So it can be easily controlled by any MPC5xxx MCU, the MPC5643L for sure. Only the driver have to be written by you. But you can find many examples for Nokia 3310 LCD handling on the web, so you can easily tailor it to your MCU.

BR, Petr

2,495件の閲覧回数
mateuszolsztyn
Contributor II

Cool, thank You very much for help. :smileyhappy:

0 件の賞賛
返信