MCAL drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCAL drivers

Jump to solution
4,859 Views
DariushTsh
Contributor III

I have MCAL drivers for MPC560 and MPC563 microcontrollers (AUTOSAR 3.0 and 4.0). Can we use them to write MCAL drivers for SPC560 and SPC563 microcontrollers?

0 Kudos
1 Solution
4,580 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Definitely you can develop for your own the AUTOSAR MCAL drivers in a NXP microcontroller. It's not mandatory to purchase the NXP AUTOSAR MCAL.

You can figure out the portfolio of our AUTOSAR MCAL here: https://www.nxp.com/design/automotive-software-and-tools/autosar:AUTOSAR-HOME

Best Regards,

Nam

View solution in original post

15 Replies
4,774 Views
namnguyenviet
NXP Employee
NXP Employee
4,798 Views
namnguyenviet
NXP Employee
NXP Employee

Hello @DariushTsh

If you're asking about the SPC560/SPC563 microcontrollers which are listed out here: https://www.nxp.com/products/processors-and-microcontrollers/power-architecture/mpc5xxx-microcontrol... and here: https://www.nxp.com/products/processors-and-microcontrollers/power-architecture/mpc5xxx-microcontrol...
Then the answer is yes, you can use the MCAL drivers for MPC560/MPC563 in those products.

Best Regards,

Nam

4,770 Views
DariushTsh
Contributor III

What MCAL drivers of NXP microcontrollers can be used for SPC563M64L5 microcontroller (of ST)?

Tags (1)
0 Kudos
4,763 Views
namnguyenviet
NXP Employee
NXP Employee

Unfortunately, there isn't any NXP MCAL drivers can be used for an ST microcontroller.

4,760 Views
DariushTsh
Contributor III

Because SPC and MPC have a common architecture, can't use each other's MCAL drivers?

But you said in this post, this is possible.

0 Kudos
4,754 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

I'm afraid you have a misunderstood. What I meant is the SPC microcontroller from NXP, not ST. Please carefully read the whole comment and check the link that I have provided, which listed out only NXP products, and not any product from ST.

Best Regards,

Nam

4,722 Views
DariushTsh
Contributor III

I'm confused.
Did I get it right ??? MPC microcontrollers can (of NXP) be used instead of SPC (of ST), but MCAL drivers of MPC microcontrollers (of NXP) can not be used for SPC microcontrollers (of ST) . Is it correct???

0 Kudos
4,716 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

If you want to integrate the NXP MCAL driver into a ST microcontroller, then you need to use with your own risks. Although the hardware might be equivalent between these two microcontrollers, it remains the fact that the NXP MCAL is only verified with NXP microcontrollers, and we can't guarantee that there wouldn't be any issue when integrating a NXP MCAL software into a ST microcontroller, or whichever another company's microcontroller.

Best Regards,

Nam

4,710 Views
DariushTsh
Contributor III

I have a general question.

Can MCAL drivers be prepared and written by software engineers and programmers at all or must they be purchased ???

Please explain about MCAL drivers and their standard

0 Kudos
4,581 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Definitely you can develop for your own the AUTOSAR MCAL drivers in a NXP microcontroller. It's not mandatory to purchase the NXP AUTOSAR MCAL.

You can figure out the portfolio of our AUTOSAR MCAL here: https://www.nxp.com/design/automotive-software-and-tools/autosar:AUTOSAR-HOME

Best Regards,

Nam

4,528 Views
DariushTsh
Contributor III

Thanks...

0 Kudos
4,749 Views
DariushTsh
Contributor III

Oh ... I'm a little confused. Can I email you or privately? Because I have many questions.

0 Kudos
4,743 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please create a ticket in here: https://support.nxp.com/s/ and our experts will be assigned to support you.

Best Regards,

Nam

4,741 Views
DariushTsh
Contributor III

Thanks ...

0 Kudos
4,780 Views
DariushTsh
Contributor III

Please help me to configure and use MCAL drivers with EB tresos Studio.

Tags (1)
0 Kudos