MCAL Example for MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCAL Example for MPC5748G

1,283件の閲覧回数
andibavaria
Contributor II

Hi,

has anyone testet the MCAL (4.0-1.0.5) example application on a MPC5748G (DevKit) lately ?

I downloaded and installed the Autosar MCAL (MPC574xB-C-G Autosar 4.0 MCAL -> SW574XG-MCAL401-RTMC_SR-1.0.5) from NXP.

The included example (MPC574XG_MCAL4_0_RTM_1_0_5_Sample_Application) is linking to a different chip version (mpc5746c). For example in the file /toolchain/Startup_vle.c i can see that "mpc5746c.h" is included. I thought it should be mpc5748g.h?

1 返信

669件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I agree with you.

Even if those are very similar chips, they are different silicons.

And they should not have common header files.

This looks like an issue of the example.

Lets see if someone from AUTOSAR team can comment on this. But best is to submit a ticket on NXP.com and then they must take care of it.

Peter