MC33908NAE and MPC5744P CAN issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33908NAE and MPC5744P CAN issue

629 Views
mayingge
Contributor II

Hi

I am working on a project  based on MC33908NAE and MPC5744P.The MC330908NAE is in the debug mode,according to  the datasheet I can use the CAN transceiver directly,but when I check CANRX,it always high, the signal from CANTX is right .And I also find that the RSTB pin of MC33908 is always low even in debug mode.

if the RSTB pin has an effect on CAN transceiver,or there is any solution for my problem?

Thanks in advance.

Labels (1)
Tags (3)
0 Kudos
1 Reply

510 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes the RSTB pin state has influence on CAN transceiver as it reset the microcontroller.

pastedImage_1.png

If it is low then your micro is in reset, and no can communication can be ongoing.

regards,

Peter

0 Kudos