MC33908 MUX_OUT question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33908 MUX_OUT question

Jump to solution
2,022 Views
shawnzhao
Contributor II

If I use IO_1 to monitor the Vcore, and config the Vcore_FB=1 in INIT VREG1 Register that means "IO_1 can NOT be used for analog/digital input neither for WU from LPOFF". Can I still monitor IO_1 from MUX_OUT by MCU if I set the AMUX0:2=110b which means selete the IO_1 to output of MUX_OUT?  Thanks!

149324_149324.PNGVcore monitor.PNG

Labels (1)
0 Kudos
Reply
1 Solution
1,931 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Shawn,

MUX_OUT output works starting minimum 3V at IO input pin. FB_core monitoring at IO_1 is 0.8V, so nothing will be measurable at MUX_OUT in that condition.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

0 Kudos
Reply
2 Replies
1,932 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Shawn,

MUX_OUT output works starting minimum 3V at IO input pin. FB_core monitoring at IO_1 is 0.8V, so nothing will be measurable at MUX_OUT in that condition.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply
1,931 Views
shawnzhao
Contributor II

Thank you, Tomas!

Yes, I find the description of the VIO, the wide range is 3~19V and tight range is 3~9V.:smileyhappy:

0 Kudos
Reply