Hi,
there's no direct support for this in Lauterbach debugger. You have to write a script which will initialize the MCU, configure the SPI and disable the watchdog via SPI. The default timeout of watchdog is 256ms, so the script must be faster...
Regards,
Lukas
Hi Lukas,
thanks for your answer. I need some more details.
For disable the WDT do you mean set the WDT window to disable?
256ms is the timeout to feed the first time the WDT, in the code I tried to disable the WDT without serving it, but the results was a reset. So is it possible do it?
Regards,
Manuela
Hi Manuela,
yes, you have to set the WDT window to disable. In order to get everything done in time, you have to use the Data.STARTUP commands. With Data.STARTUP.SEQuence you can define which values should be written to which address immediately after SYStem.Up or after Power-on (using SYStem.Mode.StandBy). You have to do everything needed to send the required SPI commands to the SBC, i.e. ME_ME, SIUL, and DSPI. to If I understand the manual correctly, the 256ms configuration time is only available after power-on, so you have to use Data.STARTUP in combination with SYStem.Mode.StandBy. Here is a templace for the setup script:
;turn off target power
SYStem.CPU MPC5643L
;set up Data.STARTUP to send the SPI commands
Data.STARTUP.SEQuence SET <addr> %<width> <value> SET <addr> %<width> <value> ....
Data.STARTUP.ON
;set up StandBy mode to connect and halt core at power-on
Break.Set 0--0xFFFFFFFF /Program /Onchip
SYStem.Mode.StandBy
;turn on target power
If everything worked well, the core should be halted at the reset address now.
See general_ref_d.pdf for details on how to use Data.STARTUP.
Best regards,
Reinhard