Yes, we can diagnose Reset activation cause:
Can we identify watchdog reset after it happens by reading WD_Answer during initialization ?
Hi,
I would read WD ANSWER register bit WD.
Peter
Hello,
We are reading bit WD in WD Answer reg to determine if there has been a reset due to watch dog not refreshed as expected. During start-up (in bootloader) we are reading the WD Answer register once. But, maybe we should do it twice? Extract from ref manual (MC33907-MC33908D2 - Rev. 5.0, 10/2016):
"Values of the three registers WD_answer, WD_counter, and DIAG_FS2 are updated at the end of any SPI access to one of these registers. To always get up to date values, it is recommended to make two consecutive SPI accesses to these registers. Example: read WD_answer, read again WD_answer, read WD_counter, read DIAG_FS2. The first read updates the three registers and the second read report the latest information".
But, the WD bit is cleared when reading it. Thus, there is a risk that the bit is set at first read and not at the second read? How should the WD bit actually be read to be sure reading the bit correct?
Best Regards,
Peder
Hi,
How about to read WD_counter in order to refresh these register status bits?
That should be sufficient in order to refresh these register values.
Peter
Hi,
Could you specify micro you are using.
Peter
Hi,
MPC5744p, is it possible to know the reset reason only from the SBC registers ?
Thanks,