Loop back for LIN bus on MPC5777M EVM board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Loop back for LIN bus on MPC5777M EVM board?

681件の閲覧回数
anishchoudhary
Contributor III

Hi,

I am testing LIN communication on MPC5777M EVM board.Here external 12V supply is necessary to test communication LIN protocol ? OR it's not necessary to supply external 12V to test LIN protocol in loop back mode ?

タグ(1)
2 返答(返信)

551件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

for internal loopback the transceiver is not used, so there is no need to supply it.

If you want to use the transceiver, then you must supply it by 12V.

BR, Petr

551件の閲覧回数
anish021
Contributor I

Hi,

For supply 12v which pin we have to use, when use GPIOs for establish connection between two LIN ports ?

0 件の賞賛