LPOFF-Sleep on MC33907

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPOFF-Sleep on MC33907

2,080 Views
chshli
Contributor II

Hello,

 

Can  the MC33907 enter in Low Power mode LPOFF - SLEEP in debug mode(entered via the DEBUG pin)?

 

Thanks

Labels (1)
4 Replies

1,810 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Li,

No, it cannot. Entering in the Low Power mode LPOFF - SLEEP is only available if the product is in Normal mode by sending a secured SPI command. 

Best regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply

1,810 Views
chshli
Contributor II

Hi Tomas,

However,according to my test,the MC33907 can enter in LPOFF-SLEEP in debug mode.

Could you make a test and tell me why?

Best regards,

Li

0 Kudos
Reply

1,810 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Li,

I have to correct my previous answer. Yes, the MC33907 can enter in the Low Power mode LPOFF - SLEEP also in the Debug mode by SPI command after closing the INIT phase of the Main state machine.

Best regards,

Tomas

1,810 Views
ramyashankar
Contributor I

What are the functionalities that can be performed while in debug mode?
1. Entering into LPOFF mode ? (Yes/No)
2. Wakeup functionality ?  (Yes/No)
3. Watchdog operation ?  (Yes/No)

Also, please I want to know whether in debug mode (entered via DEBUG pin), does SBC (MC33907) have has Init, Normal and LPOFF modes? or only under Normal operation (DEBUG pin grounded), SBC (MC33907) has Init, Normal and LPOFF modes?

0 Kudos
Reply