LIN Slave Mode In MPC5604B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN Slave Mode In MPC5604B

Jump to solution
5,157 Views
pvarela
Contributor II

I've just started with Bolero MCU. I have EVB board and I've been followed some projects from AN2865.

 

I would like configure LIN peripheral in Slave Mode receiver, but there's no example of that (there is only one Tx mode example).

 

Does anyone have some projects related?

 

Thank a lot

Labels (1)
1 Solution
4,440 Views
pvarela
Contributor II

Finally I used RAppiD_init Tool to configure LIN Slave mode in MCP5604B with Interrups, and works fine. There is one project example in path installation:

C:\Program Files (x86)\RAppID\560xB\Examples\LinflexTutorial

View solution in original post

0 Kudos
Reply
6 Replies
4,441 Views
pvarela
Contributor II

Finally I used RAppiD_init Tool to configure LIN Slave mode in MCP5604B with Interrups, and works fine. There is one project example in path installation:

C:\Program Files (x86)\RAppID\560xB\Examples\LinflexTutorial

0 Kudos
Reply
4,440 Views
andrea_mocci
Contributor II

Hi nostradamux,

I have seen RAppID linflex example; ok, it use ISR but it does not solve my problem, damnnnnn ;(...It seems that data triggering has not enough time to send all data bytes, as to say once it sends entire frame, once only BDRL.B.DATA0, once only BDRL.B.DATA0 and BDRL.B.DATA1,2, etc etc, in a totally randow way.

I do not know....

0 Kudos
Reply
4,440 Views
lama
NXP TechSupport
NXP TechSupport

I have found on my PC the code created by colleague of mine. Here is only content of main.c file.

/*******************************************************************************

* Freescale Semiconductor Inc.

* (c) Copyright 2010 Freescale Semiconductor, Inc.

* ALL RIGHTS RESERVED.

********************************************************************************

Services performed by FREESCALE in this matter are performed AS IS and without

any warranty. CUSTOMER retains the final decision relative to the total design

and functionality of the end product. FREESCALE neither guarantees nor will be

held liable by CUSTOMER for the success of this project.

FREESCALE DISCLAIMS ALL WARRANTIES, EXPRESSED, IMPLIED OR STATUTORY INCLUDING,

BUT NOT LIMITED TO, IMPLIED WARRANTY OF MERCHANTABILITY OR FITNESS FOR

A PARTICULAR PURPOSE ON ANY HARDWARE, SOFTWARE ORE ADVISE SUPPLIED

TO THE PROJECT BY FREESCALE, AND OR NAY PRODUCT RESULTING FROM FREESCALE

SERVICES. IN NO EVENT SHALL FREESCALE BE LIABLE FOR INCIDENTAL OR CONSEQUENTIAL

DAMAGES ARISING OUT OF THIS AGREEMENT.

CUSTOMER agrees to hold FREESCALE harmless against any and all claims demands

or actions by anyone on account of any damage, or injury, whether commercial,

contractual, or tortuous, rising directly or indirectly as a result

of the advise or assistance supplied CUSTOMER in connection with product,

services or goods supplied under this Agreement.

********************************************************************************

* File:             main.c

* Owner:            b08110

* Version:          1.0

* Date:             Jan-07-2011

* Classification:   General Business Information

* Brief:            LinFlex0 Lin 2.0 Slave example

********************************************************************************

* Detailed Description:

* - receive header from a LIN Master

* - either receive data from a LIN Master or transmit a data

*

*

* ------------------------------------------------------------------------------

* Test HW:  XPC560B 144 LQFP MINIMODULE, XPC56XX EVB MOTHERBOARD, PPC5604B 0M27V

* Target :  internal_RAM

* LinFlex0: Lin Slave, 19200 baudrate

* Fsys:     64 MHz PLL with 8 MHz crystal reference

*

* ------------------------------------------------------------------------------

* EVB connections and jumper configuration

*

* XPC56XX EVB MOTHERBOARD

* for LinFlex0 connection to the MC33661 LIN transceiver:

* - RXDA_SEL (near SCI !!!!) shunt over upper two pins

* - TXDA_SEL (near SCI) shunt over upper two pins

* - that is for PB2 connection to U5 and PB3 connection to U5

*

* for LIN Slave functionality

* - VSUP (J6 on the schematic) shunt disconnected

*   lin xceiver will get +12V from the Master

* - V_BUS shunt disconnected

* - MASTER_EN shunt disconnected

*

* for connection from a LIN Master

* LIN Master        Lin Slave

* +12V (VSUP) ------ VSUP pin 1 (left) (this will connect +12V from Master

*                    directly to the +12V pin of the LIN transceiver

* GND         ------ GND

* LIND        ------ upper right pin of the LIN connector when looking from

*                    outside of the board towards the board

*                           -------

                            |  |D |

                            -------

                            |  |  |

                            -------

*

* NOTE !!! this connector seems to be differently populated than

*          on the MPC5554EVB

* Thus please make sure by a electiral meter that the connecitons

* between Master and Slave are correct.

*

*

*

********************************************************************************

Revision History:

1.0     Jan-07-2011     b08110  Initial Version

*******************************************************************************/

#include "MPC5604B_M27V.h"

/*******************************************************************************

* Global variables

*******************************************************************************/

/*******************************************************************************

* Constants and macros

*******************************************************************************/

/*******************************************************************************

* Local types

*******************************************************************************/

/*******************************************************************************

* Local function prototypes

*******************************************************************************/

static void InitModesAndClks(void);

static void InitPeriClkGen(void);

static void DisableWatchdog(void);

static void InitLinFlex0(void);

static void InitHW(void);

static void InitSysclk(void);

/*******************************************************************************

* Local variables

*******************************************************************************/

static vuint32_t lin_status = 0;

static vuint32_t lin_status_old = 0;

static vuint32_t temp = 0;

static vuint32_t lin_esr = 0;

static vuint32_t lin_esr_last = 0;

static vuint32_t lin_status_last = 0;

static vuint32_t lin_bidr = 0;

static vuint32_t  rx_data[4];

/*******************************************************************************

* Local functions

*******************************************************************************/

/*******************************************************************************

Function Name : InitHW

Engineer      : b08110

Date          : Feb-11-2010

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : initialization of the hw for the purposes of this example

Issues        : NONE

*******************************************************************************/

static void InitHW(void)

{

    InitSysclk();

    InitLinFlex0();   

}

/*******************************************************************************

Function Name : InitSysclk

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : initialize Fsys 64 MHz PLL with 8 MHz crystal reference

Issues        : NONE

*******************************************************************************/

static void InitSysclk(void)

{

    InitModesAndClks();

    InitPeriClkGen();

    DisableWatchdog();

}

/*******************************************************************************

Function Name : InitModesAndClks

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : initialize Fsys 64 MHz PLL with 8 MHz crystal reference

Issues        : NONE

*******************************************************************************/

static void InitModesAndClks(void)

{

    ME.MER.R = 0x0000001D;        /* Enable DRUN, RUN0, SAFE, RESET modes */

                                  /* Initialize PLL before turning it on: */

    /* Use 1 of the next 2 lines depending on crystal frequency: */

    CGM.FMPLL_CR.R = 0x02400100; /* 8 MHz xtal: Set PLL0 to 64 MHz */  

    /*CGM.FMPLL[0].CR.R = 0x12400100;*//* 40 MHz xtal: Set PLL0 to 64 MHz */  

    ME.RUN[0].R = 0x001F0074;       /* RUN0 cfg: 16MHzIRCON,OSC0ON,PLL0ON,syclk=PLL */

    ME.RUNPC[0].R = 0x00000010;  /* Peri. Cfg. 0 settings: only run in RUN0 mode */

    /* Use the next lines as needed for MPC56xxB/S: */     

    ME.PCTL[48].R = 0x0000;         /* MPC56xxB LINFlex0: select ME.RUNPC[0] */

    ME.PCTL[68].R = 0x0000;         /* MPC56xxB/S SIUL:  select ME.RUNPC[0] */

    /* Mode Transition to enter RUN0 mode: */

    ME.MCTL.R = 0x40005AF0;         /* Enter RUN0 Mode & Key */

    ME.MCTL.R = 0x4000A50F;         /* Enter RUN0 Mode & Inverted Key */ 

    while (ME.IS.B.I_MTC != 1) {}    /* Wait for mode transition to complete */   

    ME.IS.R = 0x00000001;           /* Clear Transition flag */   

}

/*******************************************************************************

Function Name : InitPeriClkGen

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : Enable peri set 1 to be fsys div by 1

Issues        : NONE

*******************************************************************************/

static void InitPeriClkGen(void)

{

    /* Use the following code as required for MPC56xxB or MPC56xxS:*/

    CGM.SC_DC[0].R = 0x80;   /* MPC56xxB/S: Enable peri set 1 sysclk divided by 1 */

}

/*******************************************************************************

Function Name : DisableWatchdog

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : disable the watchdog

Issues        : NONE

*******************************************************************************/

static void DisableWatchdog(void)

{

    SWT.SR.R = 0x0000c520;     /* Write keys to clear soft lock bit */

    SWT.SR.R = 0x0000d928;

    SWT.CR.R = 0x8000010A;     /* Clear watchdog enable (WEN) */

}

/*******************************************************************************

Function Name : InitLinFlex0

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : Init LinFlex0 as a LIN Slave

Issues        : NONE

*******************************************************************************/

static void InitLinFlex0(void)

{

    /* enter INIT mode */

    LINFLEX_0.LINCR1.R = 0x0081; /* SLEEP=0, INIT=1 */

    /* wait for the INIT mode */

    while (0x1000 != (LINFLEX_0.LINSR.R & 0xF000)) {}

    /* configure pads */

    //SIU.PCR[18].R = 0x0604;     /* Configure pad PB2 for AF1 func: LIN0TX */

    //SIU.PCR[19].R = 0x0100;     /* Configure pad PB3 for LIN0RX */

   

    SIU.PCR[18].R = 0x0400;         /* MPC56xxB: Configure port B2 as LIN0TX */

    SIU.PCR[19].R = 0x0103;         /* MPC56xxB: Configure port B3 as LIN0RX */

    /* configure baudrate 19200 */

    /* assuming 64 MHz peripheral set 1 clock */

    LINFLEX_0.LINFBRR.R = 5;

    LINFLEX_0.LINIBRR.R = 208;

       

    LINFLEX_0.LINCR2.R = 0x20; /* clear IOBE */

   

    /* default timeout */

    LINFLEX_0.LINTCSR.R = 0;

    /* enter NORMAL mode */

    /* CCD bit 16 = 0 for checksum calculation by hardware

       CFD bit 17 = 0 for checksum field is sent after the required number

                    of data bytes is sent

       LASE bit 18 = 1 for Slave automatic resync enable

       AWUM bit 19 = 0 for The sleep mode is exited on software request

       MBL bits 20:23 = 0b0011 for 13-bit LIN Master break length

       BF bit 24 = 1 for bypass filter interrupt on ID not matching any filter

       SFTM bit 25 = 0 for Self Test mode disable

       LBKM bit 26 = 0 for Loop Back mode disable

       MME bit 27 = 0 for Slave mode

       SBDT bit 28 = 0 for 11-bit Slave Mode break threshold

       RBLM bit 29 = 0 for Receive Buffer not locked on overrun

       SLEEP bit 30 = 0

       INIT bit 31 = 0 for entering Normal mode

       =

       0x0390

     */

    LINFLEX_0.LINCR1.R = 0x2380;

   

    LINFLEX_0.BIDR.B.CCS = 0; /* enhanced checksum for LIN Slave */

}

/*******************************************************************************

Function Name : TransmitData

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : Lin Master Tx frame - example

Issues        : Not used in this example. Just a relict since the Slave code

                was started from a Master code.

*******************************************************************************/

static void TransmitData(void)

{

    /* store the data in the message buffer BDR */

   

    LINFLEX_0.BDRL.B.DATA0 = 'H';

    LINFLEX_0.BDRL.B.DATA1 = 'e';

    LINFLEX_0.BDRL.B.DATA2 = 'l';

    LINFLEX_0.BDRL.B.DATA3 = 'l';

   

    LINFLEX_0.BDRM.B.DATA4 = 'o';

    LINFLEX_0.BDRM.B.DATA5 = ' ';

    LINFLEX_0.BDRM.B.DATA6 = ',';

    LINFLEX_0.BDRM.B.DATA7 = ' ';

#if 1   

    /* Master to publish 8 bytes. ID = 0x35 */

    LINFLEX_0.BIDR.R = 0x1E35;

#else

    /* Master to send header only. ID = 0x35 */

    LINFLEX_0.BIDR.R = 0x0035;

#endif

   

    /* Trigger Frame transmission */

    LINFLEX_0.LINCR2.B.HTRQ = 1;   

   

    /* wait until Master response to the LIN header has been sent successfully */

    while(0 == LINFLEX_0.LINSR.B.DTF)

    {

        /* track LIN Status */

        temp = LINFLEX_0.LINSR.R;       

        lin_status = temp & 0x000F000;

        lin_esr = LINFLEX_0.LINESR.R;

       

        if((lin_esr & 0x00002000)==0x00002000)

        {

            /* BEF detected */

            lin_esr_last = lin_esr;

            lin_status_last = lin_status;

           

            LINFLEX_0.LINESR.R = 0x00002000;

           

            /* abort transmission */

            LINFLEX_0.LINCR2.B.ABRQ = 1;

           

            /* wait until cleared by hardware */

            while(0 != LINFLEX_0.LINCR2.B.ABRQ)

            {           

            }

           

            while(1)

            {

               

            }

        }

       

        if(lin_status > lin_status_old)

        {

            lin_status_old = lin_status;

        }

    }

   

    LINFLEX_0.LINSR.R = 0x0002; /* clear the DTF bit */

}

/*******************************************************************************

Function Name : LinSlaveReceiveHeader

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : Lin Slave - polled wait for a header and id reception.

Issues        : NONE

*******************************************************************************/

static void LinSlaveReceiveHeader(void)

{

    /* wait for LINSR[HRF] (identifier received) */

    while(0 == LINFLEX_0.LINSR.B.HRF) {}

       

    /* read the received id from BIDR */

    lin_bidr = LINFLEX_0.BIDR.R;

}

/*******************************************************************************

Function Name : LinSlaveDataReception

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : Lin Slave - data reception (subscriber)

Issues        : up to 8 bytes. for longer frames DFL>7, DBFF have to be used

*******************************************************************************/

static void LinSlaveDataReception(void)

{

    LinSlaveReceiveHeader();

   

    /* specify the data field length BIDR[DFL] */

    LINFLEX_0.BIDR.B.DFL = 0x03; /* 4 bytes - 1 */

    LINFLEX_0.BIDR.B.DIR = 0; /* BDR direction read */

   

    while(0 == LINFLEX_0.LINSR.B.DRF) {}

               

    /* read BDR registers */

    rx_data[0] = LINFLEX_0.BDRL.B.DATA0;

    rx_data[1] = LINFLEX_0.BDRL.B.DATA1;

    rx_data[2] = LINFLEX_0.BDRL.B.DATA2;

    rx_data[3] = LINFLEX_0.BDRL.B.DATA3;

   

    /* clear HRF and DRF flags */   

    LINFLEX_0.LINSR.R = 0x0005;

}

/*******************************************************************************

Function Name : LinSlaveDataTransmission

Engineer      : b08110

Date          : Jan-07-2011

Parameters    : NONE

Modifies      : NONE

Returns       : NONE

Notes         : Lin Slave - data transmission (publisher)

Issues        : up to 8 bytes. for longer frames DFL>7, DBEF have to be used

*******************************************************************************/

static void LinSlaveDataTransmission(void)

{

    static uint32_t toggle = 0;

    LinSlaveReceiveHeader();

   

    LINFLEX_0.BIDR.B.DIR = 1; /* BDR direction - write */

   

    /* fill the BDR registers */

    LINFLEX_0.BDRL.B.DATA0 = toggle;

    LINFLEX_0.BDRL.B.DATA1 = 0x55;

    LINFLEX_0.BDRL.B.DATA2 = 0xAA;

    LINFLEX_0.BDRL.B.DATA3 = 0x55;

       

    /* specify the data field length BIDR[DFL] */

    LINFLEX_0.BIDR.B.DFL = 0x03; /* 4 bytes - 1 */       

   

    /* trigger the data transmission */

    LINFLEX_0.LINCR2.B.DTRQ = 1;

   

    /* wait for data transmission complete flag */

    while(0 == LINFLEX_0.LINSR.B.DTF) {}

   

    /* clear HRF and DTF flags */   

    LINFLEX_0.LINSR.R = 0x0003;

   

    /* toggle dat for next frame */

    if(toggle==0) toggle = 1;

    else toggle = 0;

}

/*******************************************************************************

* Global functions

*******************************************************************************/

int32_t main(void)

{

    uint32_t i = 0;

    InitHW();

 

    /* Loop forever */

    for (;;)

    {

        //LinSlaveDataReception();

        LinSlaveDataTransmission();

       

        i++;

    }

}

4,440 Views
andrea_mocci
Contributor II

Hi Lad,

With few modifications, I am able to use your sample code also with an MPC5604/2 Pictus Demo board; FlexLIN interrupts are used and this represents main difference with your sample. Anyway, if I put TX/RX trip into a loop (every 150 msec, but it is just a detail), I notice that, IN THE ONLY CASE OF MPC5604P, slave response is not syncronized; sometimes it send entire response correctly, once only one byte, once 5 bytes and so on, showing a random behaviour. Using an MPC5602P Demo board all works fine.

It seems that the trigger for the data transmission (LINFLEX_0.LINCR2.B.DTRQ = 1;) does not work fine, as if queues are not well triggered (otherwise I do not understand why peripherals sends randomly correct/incorrect response).

Have you experienced anything like this?


4,440 Views
lama
NXP TechSupport
NXP TechSupport

I will try to investigate. I have found your request also in support box so I will solve it together. All further communication I will direct to support box. Ladislav.

4,440 Views
pvarela
Contributor II

Thank you!

I'm going to check it. I need some application to use this communication with INTs, but this could be first approach.

0 Kudos
Reply