Hi,
I am testing LIN Master-Slave Communication over MPC5748. I am using LINFlexD_0 as Slave and LINFlexD_2 as Master. Schematic for LIN transceiver is attached. (Note – Jumper J1 is not used)
I am using example code from - https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5748G-LINFlex-LIN-Master-Slave-test-G...
I observe that the program is infinitely stuck in the while(0 == LINFlexD_2.LINSR.B.DTF) of below function.
void TransmitData(uint16_t bidr_value)
{
/* store the data in the message buffer BDR */
LINFlexD_2.BDRL.B.DATA0 = 'H';
LINFlexD_2.BDRL.B.DATA1 = 'e';
LINFlexD_2.BDRL.B.DATA2 = 'l';
LINFlexD_2.BDRL.B.DATA3 = 'l';
LINFlexD_2.BDRM.B.DATA4 = 'o';
LINFlexD_2.BDRM.B.DATA5 = '!';
LINFlexD_2.BDRM.B.DATA6 = '!';
LINFlexD_2.BDRM.B.DATA7 = '!';
/* Master to publish x bytes with ID and CCS from bidr_value */
LINFlexD_2.BIDR.R = bidr_value;
/* Request header transmission */
LINFlexD_2.LINCR2.B.HTRQ = 1;
/* Wait for data transfer complete flag */
while(0 == LINFlexD_2.LINSR.B.DTF);
/* clear the DTF bit */
LINFlexD_2.LINSR.R = 0x0002;
}
Please advise.
Regards,
Shantanu Joshi