Many thanks for that, however the software for this forum has changed some of the text to read smiles instead it seems here:
for (; {/* Main loop */
Would you be able to upload this code some place in plain text format to avoid this ?
hi
below is the code.
#include "MPC5606B.h"
void initModesAndClock(void);
void config_PORT_E(void);
uint32_t LED_state, i;
int main (void)
{
initModesAndClock(); /* Initialisation of the device */
config_PORT_E(); /* Configuration of GPIO */
SIU.GPDO[68].B.PDO = 1; // All LEDs are off.
SIU.GPDO[69].B.PDO = 1; // -
SIU.GPDO[70].B.PDO = 1; // -
SIU.GPDO[71].B.PDO = 1; // - */
for (; :smileywink: {/* Main loop */
for (; !SIU.GPDI[65].B.PDI;){
SIU.GPDO[68].B.PDO = 0;
for (i=0; i<4500000; i++){}
SIU.GPDO[69].B.PDO = 0;
for (i=0; i<4500000; i++){}
SIU.GPDO[70].B.PDO = 0;
for (i=0; i<4500000; i++){}
SIU.GPDO[71].B.PDO = 0;
for (i=0; i<4500000; i++){}
SIU.MPGPDO[4].R = 0x0F000F00;
for (i=0; i<4500000; i++){}
}
}
}
void config_PORT_E(void)
{
SIU.PCR[68].R = 0x0200; /* LEDs are connected between PORT E pins and 5V */
SIU.PCR[69].R = 0x0200; /* PE 4 to PE 7 */
SIU.PCR[70].R = 0x0200;
SIU.PCR[71].R = 0x0200;
SIU.PCR[65].R = 0x0100; /* PE 0 */
}
void initModesAndClock(void) {
ME.MER.R = 0x0000001D; /* Enable DRUN, RUN0, SAFE, RESET modes */
CGM.FMPLL_CR.R = 0x02400100; /* 8 MHz xtal: Set PLL0 to 64 MHz */
ME.RUN[0].R = 0x001F0074; /* RUN0 config: clock selection(FMPLL) */
ME.RUNPC[1].R = 0x00000010;
ME.PCTL[68].R = 0x01; /* SIUL use the configuration of RunPC[1]
add other peripherals as needed.*/
/* Mode Transition to enter RUN0 mode: */ ME.MCTL.R = 0x40005AF0; /* Enter RUN0 Mode & Key */
ME.MCTL.R = 0x4000A50F; /* Enter RUN0 Mode & Inverted Key */
while (ME.GS.B.S_MTRANS) {} /* Wait for mode transition to complete */
}