Is the SPC5748GGK1MMJ6 pin compatible with the SPC5748GSK1MMJ6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the SPC5748GGK1MMJ6 pin compatible with the SPC5748GSK1MMJ6?

231 Views
jdseymour
Contributor I

I'm not that familiar with this family of processors.  The datasheet shows that the difference between SPC5748GSK1MMJ6 and SPC5748GGK1MMJ6 is in the "Optional fields".

My software guy tells me that this change is no problem, but I need to make sure there isn't a pin compatibility issue.  And that the "G" part is a drop-in replacement.

Can someone point me in the right direction?

Thanks.

 

0 Kudos
1 Reply

224 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If there is no conflict in used features, than yes, it is pin-to-pin compatible.

davidtosenovjan_0-1662366134431.png