Is it possible to erase BAF in MPC5748G device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to erase BAF in MPC5748G device?

Jump to solution
3,214 Views
alexvinchev
Contributor V

Hi, at our side we faced very unusual problem with the MPC5748G devices. When we were working on bootloader for these devices, somehow BAF flash area in 2 of 2 devices involved in testing got vanished (Lauterbach reads 0xFF, device stuck in reset escalation mode after boot, even if valid application is flashed).

Now I have the following questions:

  • How is this possible? We are using SSD to work with MPC5748G flash area.
  • If the above is possible, is it possible to program again this area?

We would like to recover these devices, since replacement will be long and costly, because they are on the target boards, not on EVB.

Labels (1)
1 Solution
2,422 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hello Aleksandar,

for some reasons, the BAF is not in ROM but rather in flash. I guess it could be changed in the new silicon version which should be available later this year. So, it's possible that it can be erased.

Attached you will find recovery script for Lauterbach debugger.

Regards,

Lukas

View solution in original post

5 Replies
2,422 Views
medhedibasly
Contributor III

Hello,

i'm having the same problem with MPC5748G too, i think that the BAF code area is some how erased, i'm using WinIdea and IC5000 debugger from isystem. 

is there a way to re-write that part of memory. thanks in advance.

0 Kudos
Reply
2,423 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hello Aleksandar,

for some reasons, the BAF is not in ROM but rather in flash. I guess it could be changed in the new silicon version which should be available later this year. So, it's possible that it can be erased.

Attached you will find recovery script for Lauterbach debugger.

Regards,

Lukas

2,422 Views
新股老菜
Contributor II

Hello

   The Same trouble in MCU MPC5746R,Could you help me?

0 Kudos
Reply
2,422 Views
medhedibasly
Contributor III

Hello,

try the calypsoBaf file, it should be able to recover your BAF section.

B R,

Hedi.

0 Kudos
Reply
2,422 Views
alexvinchev
Contributor V

Thank you very much Lukas!

0 Kudos
Reply