Is it able to read NVPWD register with application code only in user mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is it able to read NVPWD register with application code only in user mode?

跳至解决方案
2,007 次查看
Feiyang_Sun
Contributor II

Right now I'm using MPC56xx(SPC560P40) for a project that requires a password on OCDs which in my case is the JTAG interface. Also it requires the password "NOT READABLE OR WRITEABLE" with user codes.

Except hash the password(which I don't think make any difference since the hash operation can't be occurred after JTAG connection but before password inquire), how can I make sure that user code can't read or change the password?

标记 (4)
0 项奖励
回复
1 解答
1,994 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am not sure if I understood you correctly, but I will try to answer:

Except hash the password(which I don't think make any difference since the hash operation can't be occurred after JTAG connection but before password inquire), how can I make sure that user code can't read or change the password?

First of all SPC560P40 is device produced by STMicro and not NXP.

Second, this very old device apply only 1 protection to user code and that is censorship.

You can protect memory to be read out by setting JTAG/serial access password.

But if the application which is already in device has backdoors, it can remove/disable the censorship protection.

Have in mind that this is 20 years old design, where no security was required by customers...

In new devices, there is complex security scheme applied.

Best regards,

Peter

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,985 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, that is the case. But if you leave serial communication unprotected, what benefit will bring you locked locked JTAG?

best regards,

Peter

0 项奖励
回复
1,975 次查看
Feiyang_Sun
Contributor II

Yeah I guess that's something we need to discuss with our customers...

Anyway, thank you for your support.

0 项奖励
回复
1,995 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am not sure if I understood you correctly, but I will try to answer:

Except hash the password(which I don't think make any difference since the hash operation can't be occurred after JTAG connection but before password inquire), how can I make sure that user code can't read or change the password?

First of all SPC560P40 is device produced by STMicro and not NXP.

Second, this very old device apply only 1 protection to user code and that is censorship.

You can protect memory to be read out by setting JTAG/serial access password.

But if the application which is already in device has backdoors, it can remove/disable the censorship protection.

Have in mind that this is 20 years old design, where no security was required by customers...

In new devices, there is complex security scheme applied.

Best regards,

Peter

0 项奖励
回复
1,988 次查看
Feiyang_Sun
Contributor II

Thanks for your reply Peter.

I get what you said.

So even if I brick the ECU, which is, I'm thinking of write NVSCI0 != NVSCI1, as long as I implement the software that leaves reflash function through serial interface like LIN interface, I can still reflash that code and rewrite NVSCI0 = NVSCI1 to enable JTAG interface, is that correct?

0 项奖励
回复