Hello,
Correctable ECC Error is being injected successfully when I follow steps mentioned at 9.3 Intentional generation of FLASH 1b ECC error.
The mistake I was doing was, I was reading the FCCU Status bits from Lauterbach FCCU peripheral view. I found out that the FCCU Status register is a latch and we need to readback with the reading mode operation, only then the status bits will get updated. Now I am able to see the 1b injected ecc error in FCCU as well.
To answer your question, yes I checked reset reason when I was reading 0x00400060. It is due to reset caused by exception. Resets are happening when I try to inject multibit ecc error.
Since single bit ecc is being injected my requirement is satisfied here to monitor MEMU and FCCU path.
Thank you for the support, David