I understand, if the MACN is configured for FIFO, then the range and Mask filters can be used. Is FD supported if MCAN is configured for FIFO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I understand, if the MACN is configured for FIFO, then the range and Mask filters can be used. Is FD supported if MCAN is configured for FIFO?

1,148 Views
masoud_zahedi
Contributor I

We understand, if the MACN is configured for FIFO, then the range and Mask filters can be used.

Is FD supported if MCAN is configured for FIFO?

0 Kudos
Reply
4 Replies

1,041 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, for RXFIFO the ID range and mask can be used as well as CAN FD is supported.

BR, Petr

0 Kudos
Reply

1,041 Views
masoud_zahedi
Contributor I

Thanks a bunch Petr.

Best,

Masoud Zahedi | FAE

220 Commerce Suite 100, Irvine, CA 92602

O 949.789.4104

http://www.avnet.com<http://www.avnet.com/>;

0 Kudos
Reply

1,041 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Could you tell me which product are you using for this?

Regards,
Aldo.

0 Kudos
Reply

1,041 Views
masoud_zahedi
Contributor I

I believe the part number is MPC5777C.

Thanks

Sent with BlackBerry Work

(www.blackberry.com)

0 Kudos
Reply