I am using machine check exception to get the source of ecc error, but after one exception, second time when this exception is triggered MCAR register is not updated to the address which caused exception? Can anyone point out something I am missing ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am using machine check exception to get the source of ecc error, but after one exception, second time when this exception is triggered MCAR register is not updated to the address which caused exception? Can anyone point out something I am missing ?

1,965 Views
bilal_yousaf
Contributor I

IVOR1_Handler:
prolog_IVOR1:
e_stwu r1, -0x50(r1) # Create stack frame and store back chain
se_stw r0, 0x20(r1) # Store GPR0 (working register)
se_mfctr r0
se_stw r0, 0x10(r1) # Store CTR
mfxer r0
se_stw r0, 0x14(r1) # Store XER
mfcr r0
se_stw r0, 0x18(r1) # Store CR
se_mflr r0
se_stw r0, 0x1C(r1) # Store LR
se_stw r3, 0x24(r1) # Store GPR3
se_stw r4, 0x28(r1) # Store GPR4
se_stw r5, 0x2C(r1) # Store GPR5
se_stw r6, 0x30(r1) # Store GPR6
se_stw r7, 0x34(r1) # Store GPR7
e_stw r8, 0x38(r1) # Store GPR8
e_stw r9, 0x3C(r1) # Store GPR9
e_stw r10, 0x40(r1) # Store GPR10
e_stw r11, 0x44(r1) # Store GPR11
e_stw r12, 0x48(r1) # Store GPR12

mfmsr r0 # As function prologs/epilogs may contain
e_or2is r0, 0x0200 # SPE instruction, enable SPE, as MSR
mtmsr r0 # register is cleared at this point

e_lis r0, IVOR1_Exception_Handler@h
e_or2i r0, IVOR1_Exception_Handler@l

mtlr r0 # Store LR
se_blrl # Branch to ISR, return here

epilog_IVOR1:
se_lwz r3, 0x24(r1) # Restore GPR3
se_lwz r4, 0x28(r1) # Restore GPR4
se_lwz r5, 0x2C(r1) # Restore GPR5
se_lwz r6, 0x30(r1) # Restore GPR6
se_lwz r7, 0x34(r1) # Restore GPR7
e_lwz r8, 0x38(r1) # Restore GPR8
e_lwz r9, 0x3C(r1) # Restore GPR9
e_lwz r10, 0x40(r1) # Restore GPR10
e_lwz r11, 0x44(r1) # Restore GPR11
e_lwz r12, 0x48(r1) # Restore GPR12

mfmcsrr0 r0
e_add16i r0,r0,0x2
mtmcsrr0 r0

# mfmcsrr1 r0
# mtmsr r0

se_lwz r0, 0x10(r1)
se_mtctr r0 # Restore CTR
se_lwz r0, 0x14(r1)
mtxer r0 # Restore XER
se_lwz r0, 0x18(r1)
mtcr r0 # Restore CR
se_lwz r0, 0x1C(r1)
se_mtlr r0 # Restore LR

se_lwz r0, 0x20(r1) # Restore GPR0 (working register)
e_add16i r1, r1, 0x50 # Clean up stack

se_rfmci # Return from machine check
# rfi

2 Replies

1,486 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, quoting AN5200 section 5.1.1:

"MCSR[MAV] - indicates that the address contained in the MCAR was updated by hardware. Note that
next update is only performed when this bit is explicitly cleared by w1c operation („write 1 to clear“)."

I believe this answers your question.

https://community.nxp.com/docs/DOC-103300 

1,486 Views
bilal_yousaf
Contributor I

Thanks David. Exception Handler I was using was not clearing these bits. After Clearing these bits it is working fine now.

0 Kudos