I am looking for Fast Ethernet Controller Driver for the MPC5675K MCU.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am looking for Fast Ethernet Controller Driver for the MPC5675K MCU.

643 Views
a_tahiri
Contributor I

The FEC driver will be integrated in the LwIP TCP/IP

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

578 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you can refer to below application note and its SW package:

http://www.nxp.com/files/32bit/doc/app_note/AN4577.pdf

http://www.nxp.com/files/32bit/doc/app_note/AN4577SW.zip

FNET ethernet stack is used. There are examples for UDP, TCP/IP, web server... 

The application note is written for MPC5646C but the ethernet module is the same on MPC5675K.

BR, Petr

0 Kudos
Reply