How to use the standby in FreeRTOS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the standby in FreeRTOS?

444件の閲覧回数
1622542013
Contributor II

My program used to run in no os ;

There is a function that system goes into standby mode at a time ;

I will keep the ram unclear 0 through enable the RAM Domain Configuration Register and change the startup.c ;

Now I want to add FreeRTOS in my program;

However the standby mode is similar as RESET;

When the mcu wakes up,It will get out of the os !

How can I set the wake up address to get back into the os?

Best regards

gao

ラベル(1)
タグ(3)
0 件の賞賛
0 返答(返信)