How to use the standby in FreeRTOS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the standby in FreeRTOS?

440 Views
1622542013
Contributor II

My program used to run in no os ;

There is a function that system goes into standby mode at a time ;

I will keep the ram unclear 0 through enable the RAM Domain Configuration Register and change the startup.c ;

Now I want to add FreeRTOS in my program;

However the standby mode is similar as RESET;

When the mcu wakes up,It will get out of the os !

How can I set the wake up address to get back into the os?

Best regards

gao

Labels (1)
0 Kudos
0 Replies