Hi Everyone, I am trying to drive a valve by using eTPU functions. The main purpose is to control the duty cycle of PWM signal loaded on the valve with current control.
My way is to control PWMMDC function to output a PWM signal, which is adjusted by CC function with a ASDC function measuring current, however it did not work.
Does ASDC function need a external AD converter? or it has internal AD converter? or can I use eQADC module instead?
I have also checked the ASAC function, it seems have bit relationship with eQADC, but it confused me about how to link the eQADC and eTPU.
Appreciate your help, it would be better to example codes.
已解决! 转到解答。
Hello,
None of the eTPU functions works directly with ADC. Trigger functions for measurement of analog values as ASDC or ASAC are generating configurable trigger pulses. Which are possible connect to ADC and start the measurement.
You should separately configure ADC, eTPU does not have any internal ADC, it is pure digital IP.
These trigger functions can be used for processing of measured values, for example filtration, DC offset..
Here is a list of application notes for the functions you are mentioning:
AN2844 - using Current Controller function
AN2958 - using DC Motor Control eTPU Functions
AN2846 - using ASDC function
Here is full example project:
https://www.nxp.com/docs/en/application-note/AN3008.pdf
attached is the SW code.
best regards,
Peter
Hello,
None of the eTPU functions works directly with ADC. Trigger functions for measurement of analog values as ASDC or ASAC are generating configurable trigger pulses. Which are possible connect to ADC and start the measurement.
You should separately configure ADC, eTPU does not have any internal ADC, it is pure digital IP.
These trigger functions can be used for processing of measured values, for example filtration, DC offset..
Here is a list of application notes for the functions you are mentioning:
AN2844 - using Current Controller function
AN2958 - using DC Motor Control eTPU Functions
AN2846 - using ASDC function
Here is full example project:
https://www.nxp.com/docs/en/application-note/AN3008.pdf
attached is the SW code.
best regards,
Peter