How to use sample case 1 given by autosar_os on mpc5748g board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use sample case 1 given by autosar_os on mpc5748g board

417 Views
lubo_NEW
Contributor III

How to use sample case 1 given by autosar_os on mpc5748g board
C, OSCFG. H, and MPC574XG_AUTOSAR_OS_4_0_92_rtm_1_0_3 package AUTOSAR_OS
The original files are added to the S32DS project and are compiled with the installed DIAB compiler to generate.elf files
Readme.txt in Sample/Standard Folder But do not understand the makefile file method is OK

0 Kudos
1 Reply

408 Views
namnguyenviet
NXP Employee
NXP Employee

Please follow to the instruction in Readme file. You might need to get these SW ready before starting: EB Tresos, Make GNU, Compiler (GHS or Diab), Trace32 Lauterbach.

0 Kudos