How to use eTPUAB/C in one S32DS project at the same time? There is no distinction eTPUAB/C in all eTPU API, only use the global struct eTPU-> to operation register. So if we just modify the address highlighted below in mac5777c_vars.h, we can't use eTPUAB & C at the same time. Is there a batter way to use them at the same time?
struct eTPU_struct *eTPU = (struct eTPU_struct *)0xFFE00000; //eTPUC
uint32_t fs_etpu_code_start = 0xFFE10000;
uint32_t fs_etpu_data_ram_start = 0xFFE08000;
uint32_t fs_etpu_data_ram_end = 0xFFE08C00;
uint32_t fs_etpu_data_ram_ext = 0xFFE0C000;
Hi, please create new case according to following procedure with reference to this thread in the subject:
https://community.nxp.com/docs/DOC-329745
I am sending you example code directly as I don't want to share it here publicly.