How to set the ADC sample rate of MPC5744P?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set the ADC sample rate of MPC5744P?

1,525 Views
xuxu
Contributor II

Hi


Our project is VCU design, and we use MPC5744P as  CPU. When designing the drivers of ADCs, we found it's hard to control the sample rate.


In the MPC5744P's reference manual, it is said that ADC's highest sample rate is 1M at 80MHz. But there's no detailed description about how to config the registers to set sample rate to the  value exactly what we wanted.

sample rate.PNG
We found some  description about conversion time in the 36.5.11 of reference manual, which says the total conversion time is decided by the value of ADC_MCR[ADCLKSEL], CALBISTREG[OPMODE], CTRx[INPSAMP]. But it's confusion about the relationship between the conversion time and simple rate.

conversion time.PNG

 As the reference manual says, the smallest value of CTRx[INPSAMP] is 8, that is to say, when  CTRx[INPSAMP]=8d, the sample rate of ADC should be 1M. But if the configuration is  ADC_MCR[ADCLKSEL]=1, CALBISTREG[OPMODE]=001b, CTRx[INPSAMP]=8d, the single conversion time should be 2+8+((12+1)*4)+2=64 cycles of AD_clk, and the continuous conversion time shoude be 8+((12+1)*4)+2=62 cycles of AD_clk. So in the configuration above, the sample rate in single conversion mode and continuous conversion mode are 80/66M and 80/62M, which are larger than the highest sample rate announced.

捕获.PNG

Why?

If the relationship between the conversion time and simple rate is not Simple Rate= Frequency of ADC_CLK/Conversion time, what is the true relationship?

We did some experiments, set ADC_MCR[ADCLKSEL]=1, CALBISTREG[OPMODE]=001b, CTRx[INPSAMP]=8d, and used a signal generator to generate a 1KHz triangular wave to the ADC channel, and let the MPC5744P sampled 1000 samples from the signal, then used MATLLAB simulated the waveform, but found there were about 6 periods of triangular wave, so the sample rate calculated is 80MHz/(6*1000)=133KHz. That don't make sense.

So the question is: how to set the ADC sample rate as we wanted?

Looking forward for your response!

Thanks a lot!

Tags (2)
3 Replies

1,134 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I'll be due to minimal sample time give by datasheet that is 250*80MHz = 20 cycles

pastedImage_1.png

single conversion time = 2 + 20 + ((12 + 1) x 4) + 2 = 76 cycles what's still a bit faster

It seems the overview you have highlighted on the very top describes high accuracy mode

2 + 20 + ((13 + 1) × 4) + 2 = 80 cycles

i.e. 1 MSample/sec

1,134 Views
xuxu
Contributor II

Thanks for your answer!

If it's truly as you said,  the ST(Sample Time) must be larger than 20 cycles, then what's the point to declare the minimum acceptable value of INPSAMP is 8 ?

捕获.PNG

davidtosenovjan, I just want to konw how to control the ADC simple rate as I wanted.Is there any equations that samply tell the working principle?

Thanks.

0 Kudos
Reply

1,134 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

These are 2 different things:

- a lowest values INPSAMP that is possible to set-up (8). In this case conversion may be less accurate than specified by datasheet. For some application is may be OK, if fast conversion is the main criterion.

- a lowest values of INPSAMP that is required to choose to have set up in accordance to ADC datasheet specification to achieve specified accuracy