I'm using MPC5744p
F_VOR_FUNC
F_TSR_FUNC |
F_JTAG_FUNC
F_FCCU_SOFT
F_FCCU_HARD
F_ST_DONE
F_EXR
解決済! 解決策の投稿を見る。
Hi,
I will try to explain it.
F_VOR_FUNC - If your supply voltage get out of range and in PMC is configured to trigger functional reset on this event.
F_TSR_FUNC - Temperature sensor functional reset - when micro exceeds defined temperature ranges.
F_JTAG_FUNC - Via JTAG commands
F_FCCU_SOFT - By FCCU - when FCCU reaction on fault is configured to trigger short functional reset.
F_FCCU_HARD By FCCU - when FCCU reaction on fault is configured to trigger long functional reset.
F_ST_DONE - By micro itself after offline BIST is done.
F_EXR - External reset pin, for example reset via debugger, BCS, external watchdog, etc.
Peter
Hi,
I will try to explain it.
F_VOR_FUNC - If your supply voltage get out of range and in PMC is configured to trigger functional reset on this event.
F_TSR_FUNC - Temperature sensor functional reset - when micro exceeds defined temperature ranges.
F_JTAG_FUNC - Via JTAG commands
F_FCCU_SOFT - By FCCU - when FCCU reaction on fault is configured to trigger short functional reset.
F_FCCU_HARD By FCCU - when FCCU reaction on fault is configured to trigger long functional reset.
F_ST_DONE - By micro itself after offline BIST is done.
F_EXR - External reset pin, for example reset via debugger, BCS, external watchdog, etc.
Peter
Can you please explain me in detail how to pass JTAG commands and F_FCCU_SOFT , F_FCCU_HARD,F_ST_DONE , F_EXR
Can i have sample code regarding setting bits in FES register
Hi,
F_JTAG_FUNC - The EXTEST, HIGHZ, and CLAMP instructions cause a JTAG 'functional' reset event to occur, which sets
this field to 1.
F_FCCU_SOFT - You must set reaction on FCCU fault as short functional reset in FCCU_NCFS_CFGn register and enable reaction on this fault in FCCU_NCF_En. Then just either trigger the fault or inject it (if possible) via FCCU_NCFF register.
F_FCCU_HARD - You must set reaction on FCCU fault as long functional reset in FCCU_NCFS_CFGn register and enable reaction on this fault in FCCU_NCF_En. Then just either trigger the fault or inject it (if possible) via FCCU_NCFF register.
F_ST_DONE - Execute offline BIST. The BIST is by default enabled. If you need to configure it refer to STCU12 chapter.
F_EXR - trigger reset via external pin. Reset via debugger for example.
I hope now it is clear.
Peter
thank you peter