Hi NXP team,
The code generated by MBDT is kind of messy, which is hard to read. Therefore I tried to use only S32DS to write my code. If I choose no SDK when starting a new project like that.
I can simply ues thess codes to set the GPIO(contrl the RGB led):
to set the output:
SIUL2.MSCR[44].B.OBE=1;
SIUL2.GPDO[44].B.PDO=0;
to read the input:
SIUL2.MSCR[79].B.IBE=1;
x=SIUL2.GPDI[79].B.PDI;
However, I can't use Processor Expert to generate code until choose MPC5744P_SDK_Z4. Then the codes "SIUL2.MSCR[44].B.OBE=1;" reported errors, and only codes like following works:
PINS_DRV_SetPins(PTC, (1 << 12));
PINS_DRV_ClearPins(PTC, (1 << 12));
So I want to know whether there is a document to descript these functions in detail.