I have installed Tresos Studio 24.0 and loaded the official demo
JRE 6 and JRE 8 are not installed at the same time
Also errors like https://community.nxp.com/t5/S12-MagniV-Microcontrollers/I-have-a-problem-with-S12Z-AUTOSAR-OS-4-0-8...
已解决! 转到解答。
Hello lubo_NEW,
"[your OS folder]\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\sample\standard\sc1\src"
Then call the below command and check if it can generate configuration file successfully:
[your OS folder]\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\ssc\bin\generator\sg.exe sample1_5748G.epc
Best regards,
Hung.
Hello lubo_NEW,
"[your OS folder]\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\sample\standard\sc1\src"
Then call the below command and check if it can generate configuration file successfully:
[your OS folder]\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\ssc\bin\generator\sg.exe sample1_5748G.epc
Best regards,
Hung.