How to modify the MOSI of S32R274?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to modify the MOSI of S32R274?

1,167件の閲覧回数
donliao
Contributor II

I need to send 8 bytes command at a time, as the Correct.PNG.

But the SPI_PUSHR  can only send 2 bytes TXDATD at a time, and after the SPI_PUSHR sent the TXDATD, the MOSI will be pulled high, as the Incorrect.PNG.

Is there a way to solve the problem of MOSI pull high?

Thanks!

ラベル(1)
2 返答(返信)

1,014件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please see the reference manual chapter 57.5.4.5 Continuous Selection Format.

Peter

1,014件の閲覧回数
donliao
Contributor II

Dear Peter:

Thank you for your reply!

But the document only refers to the control of PCS, I have finished this part.

In the reference manual, the SOUT is also pulled high between the two transfers.

Is there a way let SOUT pulled low between the two transfers?

Thanks!

B.R.

Don

0 件の賞賛
返信