How can I access the device via JTAG? I have the censorship password. In Reference Manual there's only on note:
JTAG password details:
Enter password as
{NVPWD1, NVPWD0}
example –
0x89ABCDEF_01234567
But how and where should I enter it (register?) ?
Hi,
try the following process described in official Lauterbach documentation:
Regards,
Martin
This is definiteIy not a solution. This process only describes Lauterbach specific configuration. Neither does It say what the Lauterbach debugger does, nor do I have one to test it. I am using my own developed debugger and I have to add the feature to access censored devices. So what I need is the description of JTAG censorship unlocking sequence. It is mentioned but not explained in the reference manual:
Hi,
I would like to apologize for my misunderstanding.
Please look at the following app note, which should be more helpful for you.
http://cache.nxp.com/files/32bit/doc/app_note/AN4365.pdf?fsrch=1&sr=1&pageNum=1
Regards,
Martin