How to fix a bug in EB Tresos software configuration with AUTOSAR_OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fix a bug in EB Tresos software configuration with AUTOSAR_OS

3,934 Views
lubo_NEW
Contributor III

The environment is BE tresos software, configuration AUTOSAR_OS compilation error, what happened
Problem 1: Project "os_demo_sc" has errors, see Problems View
Problem 2: The external generator for module Os_TS_T2D35M4I0R92 terminated with exit code 7
Problem 3:Fails to run generator "OS_TS_T2D35M4I0R92GeneratorID" (mode: "verify") for module "OS_TS_T2D35M4I0R92"
Problem 4:Error in external generator: C:\EB\tresos\workspace\os_demo_sc\output\generated\epc\project.epc(13)
AUTOSAR/AR-PACKAGES/AR-PACKAGE[SHORT-NAME='Os']/ELEMENTS/ECUC-MODULE-CONFIGURATION-VALUES[SHORT-NAME='Os']/CONTAINERS: 3254:
Multiplicity check error for '/Os/OsAppMode'
Used generator commandline:
C:\EB\tresos\..\..\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\os_ts\eclipse\plugins\Os_TS_T2D35M4I0R92\..\..\..\..\ssc\bin\generator\sg.exe
C:\EB\tresos\workspace\os_demo_sc\output\generated\epc\project.epc

But I can use the official example of NXP to compile the past, why
Looking forward to your reply
Here are the pictures

0 Kudos
Reply
1 Reply

3,933 Views
lubo_NEW
Contributor III

NO1.pngNO2.pngNO3.pngNO4.png

0 Kudos
Reply