How to fix SZF and BEF error flags to establish communication on LIN bus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fix SZF and BEF error flags to establish communication on LIN bus?

976 Views
anishchoudhary
Contributor III

Hi,

I am working with MPC5777M EVM board for LIN protocol and for that I am configuring the GPIOs and shorting PC[9] and PC[11] pin using jumper.Find the GPIOs configuration in following attachment.After GPIO configuration I am trying to transmit data through LIN bus. But during the data transmission I found two error flag are getting set, those error flags are SZF(Stuck at Zero Flag) and BEF(Bit Error Flag). How to Fixed that error which set these error flags?

Is there external voltage is also required or not ? If it is necessary then on which GPIO pin or LIN connector port I have to give supply ?

Tags (1)
0 Kudos
Reply
1 Reply

734 Views
anishchoudhary
Contributor III

Provide external 12V supply to active the transceiver and establish proper connection.

for supply 12V on MPC5777M EVM board make connection between the P3.1 and P3.2.

0 Kudos
Reply