How to enable Freemaster CAN connection on MPC5644A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable Freemaster CAN connection on MPC5644A?

722 Views
007
Contributor II

Hello guys, as the title, can anybody help me on this? A demo project is better to show how to integrate the Freemaster serial communication SW package with a mpc5644A CAN Tx/Rx driver. I found few example codes of mpc56xx on internet. I tried Freemaster CAN connection, but failed. Just calling FMSTR_Init() in the initialization, and it needs not extra 5644A CAN initialization, is that right? 

my freemaster cfg in freemaster_cfg.h, use POLL_DRIVEN

#define FMSTR_LONG_INTR 0 /* complete message processing in interrupt */
#define FMSTR_SHORT_INTR 0 /* SCI FIFO-queuing done in interrupt */
#define FMSTR_POLL_DRIVEN 1 /* no interrupt needed, polling only */

/*****************************************************************************
* Select communication interface (SCI/FlexCAN base address)
******************************************************************************/

#define FMSTR_SCI_BASE 0xFFE40000UL /* LINFlex0 base on MPC5604B/P */
//#define FMSTR_CAN_BASE 0xFFFC0000UL /* FlexCAN0 base on MPC5604B/P */
#define FMSTR_CAN_BASE 0xFFFC4000UL /* FlexCAN_B base on MPC5644A */

#define FMSTR_DISABLE 0 /* To disable all FreeMASTER functionalities */
#define FMSTR_USE_SCI 0 /* To select SCI communication interface */
#define FMSTR_USE_FLEXCAN 1 /* To select FlexCAN communication interface */

my main() as below

int main(void)
{
volatile int counter = 0;
FMSTR_Init();

xcptn_xmpl (); /* Configure and Enable Interrupts */

/* Loop forever */
for(;;) {
counter++;
TestData1++;

if (TestData1 >= 10000)
{
TestData1 = 0;
TestData2++;
}

FMSTR_Poll();
}
}

Thanks,

hdp

0 Kudos
1 Reply

278 Views
ChenBowen
Contributor II

Do you find your answer? I am facing the same question as you had

0 Kudos