How to creating and using own Libraries with "CW for MPC55xx, MPC56xx 2.10" ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to creating and using own Libraries with "CW for MPC55xx, MPC56xx 2.10" ?

1,508 次查看
wwx
Contributor I

Requirement analysis:

Some on-board peripheral drivers in the current project need to be made in the form of (static) libraries for use by other developers.

 

The hardware platform used for project development: MPC5634M
Project development using the IDE: CW for MPC55xx, MPC56xx 2.10

 

After a few days of research, and did not find static library related options in CW for MPC55xx, MPC56xx 2.10   so I suspecte that the version is too low, then went to install CW for MCU v10.6.4, and found There is a function of making a static library, but then there is a problem that  the static library created by CW for MCU v10.6.4 , but in the CW for MPC55xx, MPC56xx 2.10 can not link it successfully.

for example:

Link Error : Linker
command file output section '.text' has a type or input which is incompatible with
section '.text' in file 'D:\Codewarrier\workspace\multiValue\Debug\Lib\mylibrary_c.obj'.
Change the type or add an input for this section.
Link failed.

 

The following questions are available:
1.CW for MPC55xx, MPC56xx 2.10 have the function of making static library? If so, where is it set up?
2.CW for MCU v10.6.4 create the library in the CW for MPC55xx, MPC56xx 2.10 that link error, how to solve.
3. What is the best solution for this requirement?

0 项奖励
回复
3 回复数

1,385 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

Your question is answered in the thread below:

https://community.nxp.com/thread/453750 

Regards,

Martin

0 项奖励
回复

1,385 次查看
wwx
Contributor I

How to use the command-Line tools  to create library?

pastedImage_1.png

Can you give me a example about it?Thank you very much.

0 项奖励
回复

1,385 次查看
wwx
Contributor I

How to use the command-Line tools  to create library?Can you give me a example about it?Thank you very much.

0 项奖励
回复