How to clear just one layer on tft

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to clear just one layer on tft

ソリューションへジャンプ
662件の閲覧回数
cedricpillet
Contributor I

Hello everyone !

I'm working on MPC560XS target with a TFT connected and i'm facing to a major issue.

I can't find a way to clear just one layer (by the 16 available with the freescale library).

 

Here is my application :

I display a picture (with Display_InitLayer() ) with 4bpp clut, and I want to make it blink as if it is a led.

But the only solution I can manage to find is to re-print all elements on the screen which make the one i'm interested to make disappear, disappear, but also all the screen because of the many texts I'm displaying.

 

 

 

Sorry if my english is not very accurate, I will do my best to make me understood.

 

Best regards.

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
598件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

If you want just “blink a layer” so the graphic, that is on this layer, disappears and appears again, it should be enough to just toggle the Layer Enable bit  (EN) of the CtrlDescLx_4 register.

Use e.g.

DCU.LAYER[0].CTRLDESCL4.B.EN = 1; and DCU.LAYER[0].CTRLDESCL4.B.EN = 0;

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
599件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

If you want just “blink a layer” so the graphic, that is on this layer, disappears and appears again, it should be enough to just toggle the Layer Enable bit  (EN) of the CtrlDescLx_4 register.

Use e.g.

DCU.LAYER[0].CTRLDESCL4.B.EN = 1; and DCU.LAYER[0].CTRLDESCL4.B.EN = 0;

BR, Petr

0 件の賞賛
598件の閲覧回数
cedricpillet
Contributor I

Hi,

Thanks for your answer.

Yes indeed I don't why I didn't manage to make it work before but now it's working.

Though I don't call the register directly but I use the macro instead provided by the freescale library which does the same.

DCU_LayerDisable(layer); which does DCU.LAYER[layer].CTRLDESCL4.B.EN = 0;

Thanks again !

have a nice day.

0 件の賞賛