How to calculate the sample time of MPC5744P ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calculate the sample time of MPC5744P ADC

Jump to solution
1,322 Views
jackjiang
Contributor II

Dears,

Datasheet page 80 have a tab for ADC parameter:

pastedImage_1.png

Reference Manual page 1060 have a sequence chart:

pastedImage_3.png

I don't understand the meaning of Sample time and Conversion time, how to explain these?

Thanks.

Labels (1)
Tags (3)
1 Solution
910 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
3 Replies
910 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is quite well described in RM section 36.5.11 Conversion time

pastedImage_1.png

In the following description there are examples for better understanding:

pastedImage_2.png

Note that DS specifies conversion time and sample time individually (as mentioned in the note below the table) thus it is needed to sum both times to get total conversion time. In other words in this table conversion time means all phase excluding sample time.

pastedImage_3.png

pastedImage_4.png

910 Views
jackjiang
Contributor II

Hi David,

Thanks for your reply.

As your say, when ADC_CLK = 80MHz(per cycle equal to 12.5ns), sample resolution is 12-bit, Tsample MIN is 250ns, so MIN sample cycles is 20d, and Tconv MIN is 650ns(MIN covnv cycles is 52d), then get the following formula:

software/hardware triggered (NSTART):
Subsequent/continuous conversion: 20 + ((12 + 1) × 4) + 2 = 20 + 52 + 2 = 74 cycles of AD_clk 

Tacd = 74 * 12.5 = 925ns, Fadc = 1s/925ns = 1.08MSPS > 1MSPS , right?

捕获1.PNG

Besides,

Why is there no ADC_CLK = 40MHz(Or other frequency) parameter for Tsample and Tconv in Table 27? because note that DS specifies "the minium value of sample time is 8".

0 Kudos
911 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Please, see following thread:

https://community.nxp.com/thread/462819