Hi:
Add a component called "flexcan" in S32DS for PA, Configuration is as follow:
MPC5748G Devkit;
Enable FD; Module clock = 80MHz; PE clock = 40MHz. using Peripheral clock
Here are my questions about the Bitrate configuration.
1) Given the values of time variables, including Propagation segment/Phase segment1/Phase segment2/Prescaler Division Factor/Resync jump width, how to calculate the sample point's value? Is there any formula for calculating the sample point's value?
2) Some sample point's values calculated by time variables are not directly available? Need to convert it to an approximation?
2) On the other hand, Given the Bitrate and sample point's value, how to calculate or select these variables?
3) Is the method used to calculate the bitrate/sample point of the Arbitration Phase consistent with that of the Data Phase?
BR,
zhou