Hello NXP community I m working on an automotive project. I m using MPC5603B,I m able to put the controller in STANDBY mode but it is not exiting STANDBY mode into DRUN mode ? How do I exit the Standby Mode ? Also how do i reduce the current consumption <1mA ?
Hi,
Look at AN4240: http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4240.pdf .
The low power modes are discussed there and a guide to create lpm application is given there too.
BR, Petr