Having trouble reading multi-channel ADC data with DMA.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Having trouble reading multi-channel ADC data with DMA.

1,381 Views
Muhammet
Contributor I

Hi,

I am using MPC5744p and having trouble reading multi-channel ADC data with DMA. When only one channel is active, I can access the data with DMA without any problems but I have problem when I try to access multiple ADC channels with multiple DMA channels. While all values written to the buffer in ram are valid when single channel is active, this is not the case in multi-channel. I shared the DMA init function and related images.
Additionally, do you have any sample codes or any documents you can recommend for using hw triggered multi-channel DMA?

exp_of_adc_prob1.png

exp_of_adc_prob2.png

  

uint32_t adc_arr2[100];
uint32_t adc_arr1[100];

static void dmamux_init(volatile struct DMAMUX_tag *dma_mux_p, uint8_t dmamux_source, uint8_t dma_ch)
{
	dma_mux_p->CHCFG[dma_ch].B.ENBL = 1;
	dma_mux_p->CHCFG[dma_ch].B.SOURCE = dmamux_source;
	dma_mux_p->CHCFG[dma_ch].B.TRIG = 0;
}

void dma_0_init(void)
{
	// DMAMUX_1 configuration for ADC trigger
	dmamux_init(&DMAMUX_1, 0xC, 1);    //dma0 channel 17 init
	dmamux_init(&DMAMUX_1, 0xC, 2);    //dma0 channel 18 init

	DMA_0.ERQ.B.ERQ17 = 1;    //The DMA request signal for channel 17
	DMA_0.ERQ.B.ERQ18 = 1;    //The DMA request signal for channel 18

	DMA_0.TCD[17].SADDR.R = ((vuint32_t) &ADC_1.CDR[1].R);    //Source Address ADC1_AN[1]
	DMA_0.TCD[17].ATTR.R = 0x0 | 0x200 | 0x0 | 0x2;    //Source transfer size 32-bit, no Address Modulo used
	DMA_0.TCD[17].SOFF.R = 0;    // TCD Signed Source Address Offset(constant)
	DMA_0.TCD[17].NBYTES.MLNO.R = 4;    //Minor Byte Count: 4byte
	DMA_0.TCD[17].SLAST.R = 0;    //TCD Last Source Address Adjustment
	DMA_0.TCD[17].DOFF.R = 4;
	DMA_0.TCD[17].DADDR.R = (vuint32_t) &adc_arr2[0];	 //Destination Address
	DMA_0.TCD[17].CITER.ELINKNO.R = 100;
	DMA_0.TCD[17].DLASTSGA.R = -400;    // Destination last address adjustment -(4byte*100 element)
	DMA_0.TCD[17].BITER.ELINKNO.R = 100;
	DMA_0.TCD[17].CSR.B.INTMAJOR = 1;
	DMA_0.TCD[17].CSR.B.DREQ = 1;

	DMA_0.TCD[18].SADDR.R = ((vuint32_t) &ADC_1.CDR[2].R);    //Source Address ADC1_AN[2]
	DMA_0.TCD[18].ATTR.R = 0x0 | 0x200 | 0x0 | 0x2;    //Source transfer size 32-bit, no Address Modulo used
	DMA_0.TCD[18].SOFF.R = 0;
	DMA_0.TCD[18].NBYTES.MLNO.R = 4;
	DMA_0.TCD[18].SLAST.R = 0;
	DMA_0.TCD[18].DOFF.R = 4;
	DMA_0.TCD[18].DADDR.R = (vuint32_t) &adc_arr1[0];	 //Destination Address
	DMA_0.TCD[18].CITER.ELINKNO.R = 100;
	DMA_0.TCD[18].DLASTSGA.R = -400;    // Destination last address adjustment
	DMA_0.TCD[18].BITER.ELINKNO.R = 100;
	DMA_0.TCD[18].CSR.B.INTMAJOR = 1;
	DMA_0.TCD[18].CSR.B.DREQ = 1;

	DMA_0.CR.R = 0xC;    //round robin is used

	INTC_0.PSR[70].R = 0x801F;    //set interrupt priority
	INTC_0.PSR[71].R = 0x801F;    //set interrupt priority
}

void dma_ch18_major_completed_isr(void)
{
	//there is a breakpoint in here to see content of the array
	DMA_0.ERQ.B.ERQ18 = 1;
	DMA_0.INT.B.INT18 = 1;
}
void dma_ch17_major_completed_isr(void)
{
	//there is a breakpoint in here to see content of the array
	DMA_0.ERQ.B.ERQ17 = 1;
	DMA_0.INT.B.INT17 = 1;
}
0 Kudos
Reply
4 Replies

1,342 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, for result draining you have to use ADC DMA source. Your configuration is incorrect.

davidtosenovjan_0-1638785223757.png

davidtosenovjan_1-1638785262923.png

 

 

0 Kudos
Reply

1,337 Views
Muhammet
Contributor I

Thanks for your feedback.

Actually, i initialized for adc1 and dma as below. Where exactly is the problem?

// DMAMUX_1 configuration for ADC trigger
dmamux_init(&DMAMUX_1, 12, 1); //ADC1 source slot 12, dma channel 17 init
dmamux_init(&DMAMUX_1, 12, 2); //ADC1 source slot 12, dma channel 18 init
0 Kudos
Reply

1,272 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am sorry, I have somehow overlooked it. This is actually right.

But you have another issue there - you cannot route one DMA source to multiple DMA channels.

davidtosenovjan_0-1639041181922.png

Use one channel for both result readings, or two linked channels, or scatter-gather feature.

 

0 Kudos
Reply

1,302 Views
kocFatma
Contributor I

I faced with same problem. I initialized DMA sucessfully. ADC works with DMA properly.

But I have trouble get DMA working from several channel. How can we achieve exact solution, could you help me for that? @davidtosenovjan @Muhammet 

0 Kudos
Reply