Generating MCAL3.0 mpc563xM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Generating MCAL3.0 mpc563xM

3,147件の閲覧回数
Ehsaaan
Contributor III

Hello Dears.

I am using EB Tresos V27.1.0 to integrate MCAL3.0 for mpc574xM. I downloaded this MCAL package from NXP.com (MPC563XM_MCAL3.0_RTM_2.0.0_signed). 

When importing this example into the EB Tresos and generate the project, it has some errors. the screenshots of errors are attached here.

By the way, this MCAL version had some Hotfixes files, for the Resource module and ADC module that I replace the old modules with them. but still, errors are remaining.

What's wrong?

 

0 件の賞賛
返信
4 返答(返信)

3,137件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan 

As the release note, this MCAL package has been tested with "Tresos 2010a.sr4 20100415-release2010a-sr4" but not tresos 27.

Could you please use the "Tresos 2010a.sr4 20100415-release2010a-sr4".

 

Module configurations were developed and tested using Tresos Configuration Tool Tresos 2010a.sr4
20100415-release2010a-sr4

Best regards,

Hung

0 件の賞賛
返信

3,129件の閲覧回数
Ehsaaan
Contributor III

Ok, thanks.

But where and how can I download this version("Tresos 2010a.sr4 20100415-release2010a-sr4") ?
Is it available on NXP.com with its evaluation license?

0 件の賞賛
返信

3,122件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

Please access the link https://www.nxp.com/webapp/swlicensing/swlicensingIntermediate.sp

hungnguyenphi_0-1623305587083.png

 

hungnguyenphi_1-1623305638720.pnghungnguyenphi_2-1623305693371.png

hungnguyenphi_3-1623305744766.png

 

Best regards,

Hung

0 件の賞賛
返信

3,118件の閲覧回数
Ehsaaan
Contributor III

Tnx a lot.
Let me check.

0 件の賞賛
返信