Will the FreeRTOS demo be updated for use with the upcoming DEVKIT-MPC5744P?
The current download only has examples for the Calypso core (T32_Calypso3M:MPC5746C and T32_Calypso6M:MPC5748G).
I can't run this demo successfully with DEVKIT-MPC5744P
my S32DS version:
S32 Design Studio for Power Architecture
Version: 2.1
Build id: 190624
The program will fly when the program start xPortStartScheduler() function.
Can you run it successfully?
Hi,
I have spoke to guys responsible for FreeRTOS.
We already have FreeRTOS ported to the PPC Z4 cores – Calypso contains Z4 cores.
The only changes needed are related to the interrupt table, memory map, and sample application.
So I expect the port will be done in future.
If you can't wait, you can do it yourself as the changes which need to be done are not anyhow complicated.
Peter
Just checking on an update to this in December 2018.
Hello Jed,
yes, there is FreeRTOS available for MPC5744P and this is part of SDK distributed with S32 Design Studio. Please see the links below:
S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released!
S32 Design Studio for Power Architecture 2017.R1 - Update 8 available
There is also example project included, which shows, how to use FreeRTOS, please see the figure below:
Regards,
Martin
When is the "Future"?
Is MPC5744P with freeRTOS finished?
Can I get the base code or model for 5744?
Any update on this? It would be very handy to have a free RTOS available for use with the MBD tools.
Thanks. The development board is still not available so it's not an immediate need.