Hi @PetrS @deepak_tech @Akhil_Karnam
Yesterday I joint the debug call with Elektrobit and this is the current situation:
Behavior:
Mother board Rev.B
Daughter board Rev.A
1. 1) J15.1 and J15.3 shorted
2) J15.2 and J15.4 shorted
3) J14 shorted
-> Notice 'Can_IsrFCA_BO' ISR triggered
No signal CANH, CANL captured on RS‑232 serial port
2. Connect J15 1-2
-> Notice 'Can_IsrFCA_BO' ISR triggered

Request from Elektrobit:
1. Recheck Daughter Board schematics for "Rev A" -> The current Daughter board Schematic you shared with Elektrobit is RevB, while the actual board is Revision A. EB would like to know if the doc can be use for their board, and is it compatible to use Daughter board Rev A and Motherboard Rev A
2. Do you have the demo code for CAN communication on this board?
They also share files include the Board image, CAN register dump before and after Can_IsrFCA_BO. if you need I can share to you in private