Flash Calibration and Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Calibration and Boot

Jump to solution
849 Views
20Sidar04
Contributor III

Dear Mr./Mrs.

When I viewed datasheet, I saw that boot and calibration example using on Flash Large Block for MPC5777C. What is purpose of boot and calibration on this flash adress?

Best Regards.

 

Flash question.jpg

 

Tags (3)
0 Kudos
Reply
1 Solution
839 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is certain use case, these blocks are not somehow special. These are just flash large block.

It is the same as blocks marked as EEPROM - these are also not EEPROM block but small flash blocks somehow suitable for EEPROM emulation.

On these device, MMU is used for remapping of address space, for calibration feature. It can be done also with other block, not only specifically with four mentioned.

View solution in original post

0 Kudos
Reply
1 Reply
840 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is certain use case, these blocks are not somehow special. These are just flash large block.

It is the same as blocks marked as EEPROM - these are also not EEPROM block but small flash blocks somehow suitable for EEPROM emulation.

On these device, MMU is used for remapping of address space, for calibration feature. It can be done also with other block, not only specifically with four mentioned.

0 Kudos
Reply